CNC Milling:
New Materials and Surface Finishes Now Available!
Take Note of Resins like PP, PPS, and PET

Last Updated: Mar 24, 2025

Four new resin materials will soon be available for CNC milling, starting December 9, 2024. Stay ahead with the latest information by exploring the use cases for each of the following!   ▶ MC Nylon (conductive, black)
  ▶ PP (standard, white)
  ▶ PPS (standard, natural color)
  ▶ PET (glass-filled, brown)

 

meviy’s CNC Milling service will introduce new annealed stainless steels and three types of surface treatments. Custom machined parts requiring surface finishes, such as low temperature black chrome, hard anodizing, and phosphate coating, can be efficiently processed from milling to surface treatment all in one place via meviy. Additionally, meviy offers AI-powered instant quoting for gold and red anodizing, which was previously limited to manual quotes. Now, you can quickly obtain pricing and delivery times for your custom parts with finishes.

Available Materials and Surface Treatments

Carbon Steel Aluminum Alloy Stainless Steel Resin

Carbon Steel

Material Surface Treatment Standard Shipping Economy Shipping
1018 Carbon Steel No Treatment 8 days 22 days
Black Oxide 10 days
Electroless Nickel
Trivalent Chromate (Clear)
Trivalent Chromate (Black)
Hard Chrome Plating (Flash Plating)
Low Temperature Black Chrome [NEW]
Phosphate coating [NEW]
1018 Carbon Steel (Polished) No Treatment 8 days 22 days
Black Oxide 10 days
Electroless Nickel
1018 Carbon Steel (Annealed) No Treatment 11 days 25 days
Black Oxide 13 days 27 days
Electroless Nickel
Trivalent Chromate (Clear)
1045 Carbon Steel (Polished) No Treatment 8 days 22 days
Black Oxide 10 days
Electroless Nickel
1049 Carbon Steel (equivalent) No Treatment 8 days 22 days
Black Oxide 10 days
Electroless Nickel
Trivalent Chromate (Clear)
Trivalent Chromate (Black)
Hard Chrome Plating (Flash Plating)
Low Temperature Black Chrome [NEW]
Phosphate coating [NEW]
1049 Carbon Steel (equivalent) (Tempered) No Treatment 11 days 25 days
Black Oxide 13 days 27 days
Electroless Nickel
Hard Chrome Plating (Flash Plating)
Trivalent Chromate (Clear)
Trivalent Chromate (Black)
Low Temperature Black Chrome [NEW]
Phosphate Coating [NEW]
NAK55 or equivalent No Treatment 8 days 22 days
4140 Alloy Steel No Treatment 8 days 22 days
Black Oxide 10 days
Electroless Nickel
Trivalent Chromate (Clear)

 

Aluminum Alloy

Material Surface Treatment Standard Shipping Economy Shipping
2017 Aluminum Alloy No Treatment 8 days 22 days
Clear Anodize 10 days 22 days
Black Anodize
Black Anodize (Matte)
Red Anodize
Gold Anodize
Hard Anodize (Clear) [NEW]
5052 Aluminum Alloy No Treatment 8 days 22 days
Clear Anodize 10 days 22 days
Black Anodize
Black Anodize (Matte)
Red Anodize
Gold Anodize
Hard Anodize (Clear) [NEW]
6061 Aluminum Alloy No Treatment 8 days 22 days
Clear Anodize 10 days 22 days
Black Anodize
Black Anodize (Matte)
Red Anodize
Gold Anodize
Hard Anodize (Clear) [NEW]
6063S Aluminum Alloy No Treatment 8 days 22 days
Clear Anodize 10 days
Black Anodize
7075 Aluminum Alloy No Treatment 8 days 22 days
Clear Anodize 10 days 22 days
Black Anodize
Black Anodize (Matte)
Red Anodize
Gold Anodize
Hard Anodize (Clear) [NEW]

 

Stainless Steel

Material Surface Treatment Standard Shipping Economy Shipping
303 Stainless Steel No Treatment 8 days 22 days
303 Stainless Steel (Annealed) [NEW] No Treatment 8 days 22 days
304 Stainless Steel No Treatment 8 days 22 days
304 Stainless Steel (Annealed) [NEW] No Treatment 8 days 22 days
304 Stainless Steel (Polished) No Treatment 8 days 22 days
316 Stainless Steel No Treatment 12 days 26 days
430 Stainless Steel No Treatment

Resin

Material Standard Shipping Economy Shipping
Acetal Standard, White 8 days 22 days
Standard, Black
MC Nylon Standard, Blue 8 days 22 days
Standard, Ivory
Conductivity, Black [NEW]
Weather Resistance, Black Ash
Polypropylene (PP) Standard, White [NEW] 8 days 22 days
Polyphenylene Sulfide (PPS) Standard, Natural Color [NEW] 8 days 22 days
polyethylene Terephthalate (PET) Glass Filled, Brown [NEW] 8 days 22 days
Bakelite Paper, Natural Color 8 days 22 days
Paper, Black
Cloth, Natural Color
Polytetrafluoroethylene (PTFE) Standard, White 8 days 22 days
UHMWPE Standard, White 8 days 22 days
Conductivity, Black
ABS Standard, Natural Color 8 days 22 days
PEEK Standard, Gray-brown 8 days 22 days

 

Use Cases

  • What is Annealing?

    Also known as “normalizing,” annealing is a heat treatment process used to soften materials and achieve uniform microstructure through slow cooling. This method effectively removes residual stresses that can cause warping or bending during machining.


303 Stainless Steel (annealed)

  • Features
    • Heat Treatment Process: Reheating to the crystallization temperature followed by slow cooling eliminates internal stresses and achieves material softening, resulting in enhanced ductility.
    • Stability in Tolerances: Compared to standard materials, this process minimizes distortion, ensuring stable tolerances after machining.
    • Machinability: Among stainless steels, this material offers superior machinability, making it ideal for complex designs.
  • Applications
    • Automotive equipment, chemical processing equipment, high-precision parts, household items, architectural elements

> See the difference between 303 and 304 stainless steel.


304 Stainless Steel (annealed)

  • Features
    • Heat Treatment Process: Reheating to the crystallization temperature followed by slow cooling eliminates internal stresses and achieves material softening, resulting in enhanced ductility.
    • Stability in Tolerances: Compared to standard materials, this process minimizes distortion, ensuring stable tolerances after machining.
    • Excellent Weldability: The annealed 304 stainless steel offers superior weldability, making it suitable for various applications.
  • Applications
    • Automotive equipment, chemical processing equipment, high-precision parts, household items, architectural elements

> See the difference between 303 and 304 stainless steel.


Hard Anodize

  • Features
    • Durable Coating: Aluminum treated with hard anodizing achieves a robust film that provides excellent wear resistance.
      *The appearance may vary depending on the material and coating thickness.
  • Applications
    • Automotive equipment, railway systems, aerospace components, medical devices

Phosphate Coating

  • Features
    • Corrosion and Wear Resistance: Phosphate coating offers excellent protection against rust and wear.
    • High Adhesion: Its strong adhesion makes it ideal for use as a pre-treatment before painting.
      * The treatment uses either zinc phosphate or manganese phosphate, resulting in variations in color and appearance. Please note that the selection of the treatment solution is not available.
  • Applications
    • Automotive equipment, industrial machinery, robotics, parts prior to painting

Low Temperature Black Chrome Plating

  • Features
    • Corrosion Protection: This surface treatment provides excellent rust and Long-lasting corrosion resistance.
    • Uniform Thin Coating: With a film thickness of approximately 2μm, it allows for high machining precision, even on treated surfaces.
    • Matte Black Finish: The matte black color helps prevent glare and reflection.
  • Applications
    • Semiconductor equipment, medical devices, optical instruments, architectural elements

MC Nylon (conductivity, black)

  • Features
    • Strength and Heat Resistance: Combines the strength and heat resistance characteristic of MC Nylon.
    • Conductivity and Anti-static: This grade nylon retains excellent conductivity and anti-static properties.
  • Applications
    • Components for electronic devices, insulation parts for electrical equipment

PP (Polypropylene)

  • Features
    • Heat and Chemical Resistance: PP is a white plastic with excellent heat and chemical resistance.
    • Cost-effectiveness: Lightweight and reasonable, making it a versatile and widely used general-purpose plastic.
  • Applications
    • Home appliances, automotive parts, packaging materials, consumables

PET (glass filled, brown)

  • Features
    • Low Water Absorption: This resin, called Unilate, is made from polyethylene terephthalate (PET) with glass fibers and inorganic fillers, offering low moisture absorption.
    • High Dimensional Stability: It offers excellent dimensional stability.
    • Machinability: Good machinability properties.
    • Electrical Insulation: Like other resins, this resin possesses electrical insulation properties.
  • Applications
    • Electrical insulation materials, semiconductor manufacturing equipment, electronic components (especially insulation parts)

PPS (standard, natural color)

  • Features
    • High Heat, Wear, and Chemical Resistance: PPS offers excellent resistance to heat, wear, and chemicals.
    • Electrical Insulation: PPS, a type of super engineer plastics, provides excellent electrical insulation properties.
    • High Dimensional Stability: Maintains dimensional stability even under harsh conditions.
    • Cost-effective: This resin is more affordable than PEEK (about 3-4 times cheaper), a similar engineering plastic.
  • Applications
    • Automotive parts (e.g., engine components), electronic device parts, precision machinery, medical devices, high-temperature parts

meviy Marketing Team

The meviy resources library is your source of information about the mechanical engineering industry. Find here all the news about materials, design tips and the latest meviy updates and release.
Follow MISUMI USA