Four Common Surface Finishes

Last Updated: Nov 06, 2024

A photo of car body painted red

Surface treatments are one of the finishing methods used in material processing. Unlike machining or injection molding, surface finishes do not change the shape of the material itself, but they play a critical role in enhancing the material’s properties. This article explores the types and processes of common surface finishes.

What is Surface Finish?

Surface finishes and surface treatments, as the term implies, are finishing processes applied to the outer surface of a material. For example, a resin or metal surface is painted or plated to prevent the rusting of sheet metal or to achieve a better product appearance.
These procedures include both additive processes, where additional substances are added to the surface of a material, and ablative processes, where a small portion of the material’s surface is removed.

Common Surface Finishes

Processes that Attach Material to the Surface

Painting and Coating
Covering a material with a layer of paint protects it from corrosion. Paints with a wide range of colors make it possible to cover materials to improve their appearance. Paint can be applied to both metal and plastic surfaces.
You may have seen imprints, such as a manufacturer’s logo, on appliances. This is another type of coating. Painted products are used in a variety of applications, including car bodies, outdoor signs, and appliance housings.
There are two primary methods of painting: spray painting and electrocoating, which uses an electrolytic solution within the dissolved paint.

A component paintned yellow

Plating
Plating is the application of a thin layer of metal to the surface of a material. In the past, plating was only applied to metals, but advancements in technology have made it possible to plate resins as well. The main purpose is to prevent rust and corrosion, and to improve appearance. Plating is also commonly used as a finishing technique to cover the exterior of products using expensive and beautiful-looking metals such as gold.
In addition, many products, such as grates and screws, which appear to be entirely steel are actually galvanized or otherwise plated.
Known plating processes include hot-dip plating, which involves immersion in molten metal, chemical plating, which deposits ionic metal on the surface, and electroplating.

Processes that Remove a Small Portion of the Surface

Polishing
Polishing is a process used to make surfaces smooth. This can be done not only by scraping the surface with brushes or abrasives, but also by using polishing chemicals that slightly dissolve the surface, or by electropolishing, which involves dissolving the surface using an electric current in a solution. Polishing removes impurities like oxides and foreign materials, reducing small surface imperfections. It also improves the surface’s appearance and makes it more resistant to friction when in contact with other parts. This finish is often used to create metal components with a mirror-like finish.

Cleaning
Cleaning involves removing unwanted substances from a material’s surface. This can be done by washing with water or detergents, or by using other methods like barrel processing, which mixes the material with abrasives, blasting, which sprays it with metal or abrasive particles, and honing. The primary goal is to get rid of foreign materials and impurities, such as oxides. Barrel and blasting processes are also commonly used to remove burrs after machining. Additionally, parts that have been cut or machined often have coolant or lubricants on them, making cleaning necessary. Some metal parts with a texture known as “orange peel” may also be cleaned using blasting.

Large wash machines for cleaning components

Conclusion

Many metal products we use commonplace in our daily lives have undergone some form of surface treatment. By examining the parts and products around you and considering what types of surface treatments they may have undergone, you can gain a deeper understanding of surface processing.


What’s meviy?

On-demand, fast sourcing of quality custom mechanical parts is made possible by meviy.

meviy is one of the most reliable on-demand manufacturing platforms in the US that allows you to get instant quotes for your mechanical parts simply by uploading 3D CAD data. No longer need to create 2D drawings just to quote parts. This platform supports not only manufacturing but also common surface finishes for sheet metal fabrication and CNC machining, including milling and turning, and has saved time for over 160,000 mechanical designers and purchasers worldwide.

meviy’s Surface Finishes

Sheet Metal
A yellow painted part for sheet metal

 

Learn More

CNC Milling
A black anodized aluminum part for CNC Milling

 

Learn More

CNC Turning

A rod shape shaft for CNC Turning

 

Learn More

 

meviy Marketing Team

The meviy resources library is your source of information about the mechanical engineering industry. Find here all the news about materials, design tips and the latest meviy updates and release.
Follow MISUMI USA