How to Use the 3D Viewer

(1) Toolbar

(2) Cube

(3) Display Settings

(4) PMI

(1) Toolbar

The names of each tool and what you can do with these tools are specified below.
Function Name What You Can Do
Designate Design Origin
Move the design’s origin point. → Change a Design’s Origin
Add Dimensions
Add dimensions and dimensional tolerances. → Add/Remove Dimensions and Dimensional Tolerances
Add Dimensions in Batch
Batch add coordinate dimensions. → Adding Dimensions*No dimensions will be added to faces which are at an oblique angle.
Delete PMI
Remove added dimensions. → Add/Remove Dimensions and Dimensional Tolerances
Hide dimensions
Hides dimensional tolerances guaranteed by “Default General Tolerance Standards for Machined Dimensions.”
Split Grouped Holes
You can split holes grouped during shape recognition. → Splitting Grouped Holes
Function Name What You Can Do
Set Surface Roughness
Surface roughness can be set. → Set Surface Roughness
  • Datum
Datum can be set. → Set datum and geometric tolerances
  • Geometric Tolerance
Geometric Tolerance can be set. → Set datum and geometric tolerances
  • Engraving
Add engraving. → Set engraving
Measurement
This function allows measurement of models uploaded. → Measuring 3D models
Change Font Size
You can change the font size of the PMI display. → Changing Font Sizes
Simple 2D Drawing
Download image files that capture each orthogonal direction of the 3D models and arrange them via 3rd angle projection.

(2) Cube

  • Rotate the cube to change the orientation of the currently displayed parts.
  • Click [Isometric View] to return to the isometric view (default orientation).

(3) Display Settings

  • Move the mouse over the icon to display the display settings menu.
  • Here you can change the 3D model display method, and also toggle between displaying or hiding text information in the 3D viewer.

(4) PMI

PMI is an abbreviation of Product Manufacturing Information and refers to textual information for dimensions and holes. The position of the PMI display can be moved by dragging.

Recently viewed articles