Set engraving
How to set up engraving
STEP1 Select icon
- Select the icon from the icons at the top.
- You can also use the shortcut key (E).
STEP2 Engraving surface selection
- Select the surface you want to engrave.
- When you hover the cursor over a selectable surface, the surface is highlighted.
STEP3 Engraving specification setting
- Enter the text you wish to engrave.
- To specify part number engraving, click “Add Part Number”. A temporary part number (MVBLK-XXX-XXX-XXX-XXX) will be issued and displayed in the 3D Viewer.
- The position can be moved within the area of the face, along with specifying the text size and angle. After specifying, click “Update”.
Caution
Characters that can be entered in the dialog are single-byte alphanumeric characters and some symbols (+-. #$%&()=*:? /_~).The complete part number will be displayed after you click “Confirm the quotation conditions”.
STEP4 Completion of engraving setup
You can see the set engraving on the 3D Viewer model and in the tree view.
How to delete
STEP1 Select icon
- Select the icon from the icons at the top.
- You can also use the shortcut key (D).
STEP2 Select engraving
- The message “Click on the PMI you want to delete.” will be displayed, then
select the engraving you want to delete. When the cursor is over an engrave, the corresponding engrave will glow blue. - Clicking will delete it.
Caution
Please note that clicking the “Delete all PMI” button will delete all PMIs you have set.STEP3 Finish deleting
Deletion completed.
STEP4 End of dimension deletion
Press the Esc key or the X button to exit Delete PMI.