Shipping Days
- Orders placed within the cutoff time will be counted starting from the next business day. (Saturdays, Sundays, and holidays are not counted.)
- *Delivery times may be longer than usual during extended holidays.
- The shipping dates for auto-quoted items are as follows. The shipping date varies depending on the quantity ordered.
- *For Welded Sheet Metal services, extended lead times are available in addition to standard shipping dates. Please refer to the “Delivery Options” for details.
- *For details on welding types and finishing methods, please refer to “Instructions and Details for Welding Information“.
| Material: Ferrous Metals | Surface Treatment | Standard Shipping | Economy Shipping* | ||
|---|---|---|---|---|---|
Standard Welding: Arc welding, laser welding | Spot welding only | Standard Welding: Arc welding, laser welding Spot welding | |||
Welding finish: Burn Mark Removal Only | Weld finishing: Grinder finishing | ||||
| Low Carbon Steel (Cold/Hot Rolled) | - | 8 days~ | 9 days~ | 7 days~ | 22 days~ |
| Powder Coating* | - | 11 days~ | 9 days~ | 27 days~ | |
| Wet Paint* | 12 days~ | 10 days~ | |||
| Electroless Nickel Plating | 10 days | 11 days~ | 9 days~ | 27 days~ | |
| Black Oxide | |||||
| Trivalent chromate (Clear) | |||||
| Trivalent chromate (Black) | - | - | |||
| Low Carbon Steel (Hot Rolled)* | - | 9 days~ | 10 days~ | - | 22 days~ |
| Powder coating* | - | 12 days~ | - | 27 days~ | |
| Electroless Nickel Plating | 11 days~ | 12 days~ | - | 27 days~ | |
| Black Oxide | - | ||||
| Trivalent Chromate (Clear) | - | ||||
Low Carbon Steel (Cold Rolled) | Electrolytic Zinc Plating | 8 days | - | 7 days | 22 days~ |
| Material: Stainless steel | Finishing Method | Standard Shipping | Economy Shipping * | ||
|---|---|---|---|---|---|
| Standard Welding:
Arc welding, laser welding |
Spot welding only |
Standard Welding:
Arc welding, laser welding
Spot welding |
|||
| Welding finish:
Burn Mark Removal Only |
Weld finishing:
Grinder finishing |
||||
| 304 Stainless Steel | No.1 | 8 days~ | 9 days~ | - | - |
| 2B | 7days | 22 days~ | |||
| Single-Sided #400-Grit Polished | - | - | |||
| 430 Stainless Steel | 2B | 7 days~ | 22 days~ | ||
| Material: Aluminum | Surface Treatment | Standard Shipping | Economy Shipping * | ||
|---|---|---|---|---|---|
| Standard Welding:
Arc welding, laser welding |
Spot welding only |
Standard Welding:
Arc welding, laser welding
Spot welding |
|||
| Welding finish:
Burn Mark Removal Only |
Welding finishing:
Grinder finishing |
||||
| 5052 Aluminum Alloy | - | 8 days~ | 9 days~ | 7 days~ | 22 days~ |
| Clear Anodize | 10 days~ | 11 days~ | - | 27 days~ | |
| Black Anodize | |||||
| Black Anodize (matte) | |||||
- * Due to manufacturing constraints, Low Carbon Steel (Cold/Hot Rolled) sheet thicknesses of 6mm will have one day added to the standard shipping date.
-
* Powder-coated products listed below will have the number of days indicated in the standard shipping date added.・Items with thicknesses of 6mm or greater and approximate Munsell values N1, N9.5, 2.5Y8/14, 5Y7/1: 2 days added・Approximate Munsell values 5Y7.2/1.4, 5P9/1 for all plate thicknesses : 3 days added
- * If the order includes R-bend shapes, 1 to 2 days will be added to the standard shipping date.
- * If nut installation is included, add 1-2 days to the standard shipping date.
- * If two or more plate thicknesses are required, add 1 day to the standard shipping date.
- * For welded heavy items (total of three sides: length, width, height exceeds 1500mm, or weight exceeds 20kg), add 1 day to the standard shipping date.
- * For Economy lead time service, the following are excluded: Steel (untreated) over 9mm, certain painted items (powder coating in 2 colors (approximate Munsell values: 5Y7.2/1.4, 5P9/1)), 304 Stainless Steel (NO.1), and 304 Stainless Steel (Single-Sided #400-Grit Polished) are excluded.
- * Depending on the delivery type, slight color variations may occur in the appearance of plated items. If you wish to standardize the color, please specify in the comments section (Other Additional Instructions) and request a quote from meviy Support.